This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS549D22: Thermal Simulation of IC-Die vs IC-TOP

Part Number: TPS549D22


Hi TI expert,

My team is current using TPS549D22 for a new project design. The application is as below.

1> Vin=12V(+/-5%)

2> Vout=3.3V

3> Iout=23.5A

There are three questions.

1. We do the test with Fsw=600Khz and Fsw=400Khz. The efficiency is 93%@600Khz, 23.5A, and 93.3%@400Khz,23.5A. Seems the efficiency is just affected a little by the switching frequency change. Could you explain the reason?

2. Per the thermal image test under 25 ambient, no airflow(18layers PCB), the hottest top case temperature of IC is 75.6 deg.C(600Khz, max load). How to calculate the junction temperature?

3. Per using TI Webench, the simulation result shows the efficiency can be 95%+. The IC power dissipation is 3.15W. And IC- Top is 60.6 deg.C and IC- die is 57 deg.C. Does this mean IC junction temperature is even lower than the IC top case temperature? 

For our motherboard design, we usually have 18 layers or 20 layers PCB. The PCB can provide very good thermal dissipation path. But in our main board, the ambient temperature is not possible to be 25 deg.C. It may be as high as 55 deg.C to 60 deg.C because the air is preheated by the CPU or the switch chipsets.

Look forward to your comments.

Thanks,

Dora