Hi, Team
My customer Hytera feedback that when they are using BQ25895, they found a problem doesn't match with datasheet.
If we set BQ25895 in Boost mode, PMID outputs 5V.
Then battery voltage drops eventually, if VBAT gets VBAT_OTG, about 2.85V, BQ25895 will exit boost mode as expected, but it will also turn off Q4, VSYS will lost the power from battery.
If we don't set it in boost mode, it will turn off Q4 until 2.2V which is as expected from datasheet description.
I test it in a BQ25895EVM, it works the same as customer's board.
Meanwhile, I verified this test in a BQ25892EVM, it will not turn off VSYS when VBAT drops <VBAT_OTG.
Can you please kindly help to check if this is a known issue?
What's our solution to solve it?
Any other parts to replace BQ25895?