Other Parts Discussed in Thread: TLC5943
you can change the program that starts when you turn the plate tlc5943evm-274?
is written to the eeprom instead of the 16 rotating colors such as blue green red or any other modified by the user?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLC5943
you can change the program that starts when you turn the plate tlc5943evm-274?
is written to the eeprom instead of the 16 rotating colors such as blue green red or any other modified by the user?
thanks
Hello Alex,
Do I understand right that you want to change the colors directly after startup of the software? You can load the pattern you want directly after startup of the board. If you do not want the default values to appear on the EVM, you could maybe hold BLANK high until you loaded your pattern and then release the BLANK signal.
In your application, you can start the TLC5943 with any pattern that you need.
Best regards,
Brigitte
aver if I had understood correctly ... I want to know is if you can change the default pattern is the pattern that starts when you turn the plate without the words usb connect patter that stored in the EEPROM of the board and nothing else gets turned on by default in this case is 16 rotating colors I want to know if I can make after turning on the plate rather than charge a pattern that own or one that is already created using the software that came with it, idk if you have to burn eeprom with an eeprom recording program or can be done with the program itself that comes with the component