Hi
We have an existing design based on LM5071 and the DA2257 transformer to give a 3V3 output, based on the AN1430 app note, fig 12.
We now want to add a 5V5 rail by using Sec2 from T1 (pins 6 & 10).
We built it, and it does give a 5.6V output, but the output at J6 seems to be only regulated by zener Z4 - if we remove the zener the voltage at J6 is 11V, even though the voltage at J4 is 3V3.
This means the Z4 is constantly conducting, pulling around 18mA.
Is this expected, or have we done something wrong?