Dears:
From the datasheet we can see the the Current Limit information, and there are two issues about it.
1. Is there any formula about Current Limit and VIN/VOUT? For example, if we want to know the value of Current Limit under VIN is 5V and VOUT is 3.3V, how can we get the value?
2. What is the means about Not production tested? Is the value is only evaluated?
Pls. kindly help to give some advice.