This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS560430: Inverting DCDC using TPS560430

Part Number: TPS560430


Hi all

Would you mind if we ask TPS560430.

The customer plans to configure inverting DCDC using TPS560430.
Input : 12V
Output : -15V/0.3A(max)

So, we would like to calculate Cout and L, do you have some documents to calculate it?
Should we refer to following document?
http://www.ti.com/lit/an/snva722b/snva722b.pdf

Kind regards,

Hirotaka Matsumoto