This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54360: Common Ground?

Part Number: TPS54360

Hello Sir,

I am designing a power rail where I have multiple power rails.

1V, 1.2V, 1.8V, 3.3V etc. 

plus I have operational amplifiers on my board for which I need a dual supply (+-12V, +-7.5V).

I want to to know how ground connections are done?

means I have to connect all power rails ground to (negative supplies ground?).

please clarify this and please share some regulators which can give (+-12V, +-7.5V). supply with very less ripple.

Thanks and Regards

Vishal Kakade