This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692-Q1: Bandwidth of IMON pin signal with a 1nF capacitor connected

Part Number: TPS92692-Q1
Other Parts Discussed in Thread: TPS92692

Hi 

I have a question regarding to the external capacitor connected to the IMON pin. 

In the datasheet, it is said that IMON pin could "report the instantaneous status of LED current measured by the rail-to-rail current sense amplifier." Based on this information, if a 1nF is connected, whats the bandwidth of the signal of IMON pin? 

If I want to do an precise sampleing of the IMON signal, do I need to change it into a smaller cap?

Best Regards, 

Kevin