This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145: LM5145 constant current control loop

Part Number: LM5145
Other Parts Discussed in Thread: LM5176

I need Power supply  LM5145  with adjustable output voltage and adjustable output current , that is, CV  loop and CC  loop too.

I'm thinking how to add CC loop.

I noticed, lm5176 has internal CC loop  implemented so that CC error amplifier discharge soft start capacitor on SS input.

Can I use a similar principle with LM5145?
External error amplifier,  over diode and resistor discharge soft start capacitor on SS input.
Or, it is better to use it
ÏLIM input
or
COMP Output, which is output of FB error ampélifier and input PWM Comparátor at the same time.?

Thank you for the advice.