This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202: External LC parts reduction possibility

Part Number: TPS54202


Hello application team,

I'm considering TPS54202 proposal for my client.
To pursue both the space and the system cost reduction, I'd like to know how much the possible reduction range of external inductor(L) and output capacitor(Cout) value. Could you instruct it with the following conditions?

Vin=24V, Vout=12V, Iout=0.2A

The output ripple is not large concern since it has LDO for the final output.

Some performance can be degraded unless the loop stability gets unstable.

Thanks in advance.

Shinya Sawamoto

TI Japan East area FAE