Hello,
I look for power switch product which two power input, one output.
One input is 5V like USB power. Another is 12V or 5V, depends on the cases.
Is there a product which above two rail can switch? I think there is no current information but it would be helpful for example.
So far, my idea is two TPS25940 and one transistor for disabling 5V efuse when 12Vin applied.
Best regards,
Toshihiro Watanabe