Dear Specialists,
MY customer is considering TPS65381A-Q1 and has inquries.
I would be grateful if you could advise.
---
I'd like to know the operation of ENDRV in the state diagram of "VDD 5, VDD 3/5 or VDD 1 Overvoltage Condition" in the datasheet Figure 5-15.
According to the description,
The ENDRV is turned off once after detection of abnormality, and then it is restarted.
Is it necessary to set the ENABLE_DRV bit to 1 again after recovering from error?
(In this case, bit at bit error is cleared to 0?)
Or, if ENABLE_DRV was originally set to 1, as it is after return from abnormality
ENDRV turns ON even if it does.
On the other hand, in the Diagnostic mode, if ENDRV is set to ON, even if the WD abnormality occurs, it switches automatically from OFF to ON after returning.
What happens in the case of Active State?
Will it be possible to prevent ENDRV from returning to H if it shifts to Safe mode after detection of abnormality?
---
I appreciate your great help in advance.
Best regards,
Shinichi