Hi
Our customer requests information of number of flow and reflow.
Do you have these information about LM317KRRT?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Na,
We qualify our packages for MSL per JEDEC J-STD-020 which specifies that the parts run through 3 reflows. It is possible to access the JEDEC specification if you have a registered account with JEDEC. As JEDEC owns the material the customer should register with them in order to view the reflow environment and process.
I believe that you have a typo in the package and meant to refer to the KTT package. Per the Package Option Addendum which is appended to the end of the datasheet this package is rated the following:
Very Respectfully,
Ryan