This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76003: Oscillator spec

Genius 17325 points
Part Number: LM76003

Hello,

 

I have a question, just confirmation, for LM76003 oscillator spec.

The datasheet defines the condition of “Minimum adjustable frequency by R_T or SYNC” as RT=133KOhm with 0.1%.

 

Is it impossible to use 133Kohm with 2% or 0.5% instead of 0.1%?

I understand the oscillation frequency could be less than 270KHz with 2% or 0.5% resistance, but if it is no problem I want to consider to use it.

 

Also if it is no problem, could you tell me MIN oscillation frequency with 133Kohm with 0.5% or 2%?

 

Regards,

Oba

  • Hi Oba,

    Yes you can use a higher tolerance resistor for the RT set frequency. It is just the value on the datasheet is guaranteed using the 0.1% resistor.
    Therefore you can expect a larger deviation with a higher tolerance frequency. Unfortunately we do not have the data using a higher tolerance resistor. But maybe you can have some approximation from equation 6 in the datasheet
    www.ti.com/.../lm76003.pdf

    I hope that helps
    Thanks
    -Arief
  • Hello Arief,

    Thanks for your reply.
    This is just confirmation.
    Can we guarantee all operation except for oscillation frequency with 133KOhm+-2%?
    How much tolerance of resistor can be allowed for 133KOhm?
    I mean how to think about the largest resistance value (means lowest frequency) that can be connected?

    Also regarding min frequency when using 133KOhm+-2%,

    From equation 6 in the datasheet,
    Frequency = 38400/Rt - 14.33

    When 133K(0.1%), the frequency = 302.763 - 303.341KHz. From the datasheet, we guarantee 270-330KHz in this case.
    When 133K(2%), the frequency = 297.391 - 308.944KHz. So 297.391 * (270/302.763) = 265.209 KHz. This value may be min frequency.
    Does this make sense?

    Regards,
    Oba

  • Hi Oba,

    Normally i just use a 1% resistor into the RT. If you like a tighter tolerance maybe you can use the SYNC.
    All of our bench validation for this part is done with 1% resistor, therefore for operational purpose there should be no issue with using a 1% resistor in this case.

    The guarantee spec is only if you use the 0.1% resistor as shown on the EC table and this spec is over temperature.

    The equation is used only for approximation and i think it is only for room temperature.

    I hope that helps

    Thanks
    -Arief
  • Hello Arief

    Thanks.

    I’m a little bit confused about what we guarantee.

    I think there are two different things.

    One is only oscillator itself. It means just guarantee for oscillation frequency.

    I understand oscillation “frequency” can be only guaranteed with 133Kohm+-0.1%.

    0.5% or 2% can be used for Rt but we don’t know the oscillation frequency with them.  I think I understand it.

    The other is whole device operation.

    This is my unclear point. My concern is especially minimum frequency that we can guarantee whole device operation. The data sheet said that this device support only over 300MHz operation. Actually 270MHz  seemed be accepted.But how about under 270MHz? With 2% Rt resistor, it may be under 270MHz. Can we guarantee the device operation with it?

    I would like to know especially 2% case. I understand we don’t know the exact osicillation frequency, but can we guarantee the device operation in this case?

    Regards,

    Oba

  • Hi,

    We will continue the discussion through email, therefore i will close this thread for now

    Thanks
    -Arief