This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV759P: Load Transient Response Curve

Part Number: TLV759P

Hi,

I am searching through TLV759P spec, and understand this device provides fast line and load transient performance.

Do you have any load transient performance measurement curve from 0 --> 1A? Please advise.

Thanks,

Philip

  • Hi Philip,

    This device is still in preview stage and limited data has been published with the current  datasheet. Once it gets to RTM, we will have load transients curves in the final datasheet. I do have some curves that I have collected during initial evaluation that I can share to you.

    Here is the load transient performance for this device under the following conditions:

    Vin = 3.8V, Vout = 3.3V, current rising/falling slew rate 1A/us from 1mA -> 1A, Cin=Cout =1uF

    Regards,

    Jason Song