Hello Team,
My customer intend to use TPS715 for 24V to 5V_20mA, which has power loss 0.38W, since TPS715 is a SC70 package, can you tell if 0.38W for SC70 package is OK? or not recommended? in a case of 25C room temperature, what about the Tj looks like? is it possible to predict the thermal condition before customer use it to do the real test?
Thanks,
Martin