Other Parts Discussed in Thread: BQ78350, BQ76930, BQSTUDIO
After months of it working, the bq78350 seems to stop working. Here is the data Iv'e acquired so far:
1) bq76930 REGOUT pin is at 2.5V.
2) After button press TS1 is pulled up to 2.7V to boot AFE.
3) I see the usual change in current from 15mA to 18mA so AFE seems to boot okay.
4) PRES is pulled low.
5) KEYIN is pulled low.
6) MRST is pulled high.
7) Once VCC is applied VEN stays high and does not pulse.
8) No activity on I2C bus... it stays high.
9) PWRM stays high 1.76V (On working boards this voltage is the same but it only stays high if SMBUS is communicating).
10) ALERT goes high and stays high (On the working boards we have ALERT pulses every 1/4 second about 10-20 times or so).
Data point 10 has me worried because I thought any ALERT issue would be an "AFE thing".
Also... the board and battery is sealed in an enclosure. There is not contact with the board and we have ESD protection on the pins of the only exposed header.
It's is essential for us to pinpoint the source of the failure and why it failed because this is for a drone application.
Thanks guys,
JP
UPDATE: The alert pin is definitely and output of the AFE, I raised the pin from the board and tested the pin separately from the trace and it goes and stays high after boot.