This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VCSEL LED Driver

Other Parts Discussed in Thread: TPS92515

Now I have a project wnat to use VCSEL LED(see the spec below), input 5V, and control it on for 3ms, off-60ms, on-3ms, off-60ms......

I'm not sure what kind of LED driver I should use. Due to the end device is mobilephone, there is size limitation.

1. Power module: But the FB voltage is too big to do constat current.

2. Illumination Driver: Like TPS92515, but it needs external diode and inductor, the board size is big.

3. Flash LED driver: I'm not sure Flash LED driver could handle such frequent on-off cycle.

PS. The drivering current could up to 3A, it's kind of Laser LED. Based on driver solution, maybe the current spec could modify, but 1.5A at least.

Could you please help to advise any component? Thank you.