This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24161B: 3.5A Dual input battery manager that can work with no battery connected

Part Number: BQ24161B

Hello,

For a project, I need to find a battery manager that :

  • Can output 3.5 A to system/battery.
  • Works with Li-Po battery or LiFePO4 battery (it can be a different chip)
  • Can limit battery charge current according to the system load to let system works at full power.
  • Accepts a 5V Wall input (3.5A)
  • Accepts a 5V USB input (up to 3A, USB-C)
  • Can work with no battery connected
  • Can automatically switch from Wall to USB if wall is disconnected, with no interruption of the output, even if no battery is connected
  • Can automatically switch from USB to Wall if wall is reconnected, with no interruption of the output, even if no battery is connected
  • Can be monitored by I²C (or SPI)

Do you have such a device ?

Many thanks