This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2115A: Solutions to replace BD2204GUL-E2

Part Number: TPS2115A
Other Parts Discussed in Thread: TPS22912C, TPS22910A

Hi Team,

Does TI have solution to replace BD2204GUL-E2? One of the supply rails is 1.8V.

Thanks a lot.

Vincent Chen 

  • Hi Vincent,

    Our closest, simplest solution is using the TPS22912C and TPS22910A as described in the application note below (section 2).

    To suggest other possible solutions, it would also be helpful to know the following:

    1. What two voltages are being muxed together?
    2. What current rating is needed?
    3. Can the output voltage drop when switching supplies?
    4. In general, what kind of an application is this?

    Thanks,

    Alek Kaknevicius