Other Parts Discussed in Thread: TPS62100
Tool/software: WEBENCH® Design Tools
Hi
It was failed when I check this device to operate for the following condition by WEBENCH. Because of current limit and duty cycle limit.
Condition; Vi=1.5V, Vo=4.2V, Io=0.2A
Then I checked the datasheet and the current limit which is minimum value is 1.2A.
So the simulation result is smaller than spec.
Why is this device not possible to use for the above condition?
Best Regards,
Koji Hamamoto