Other Parts Discussed in Thread: PMP10215
Dear Team,
My customer is design one AC-DC power board based on LM5021MM-2/NOPB . The topology is two-transistor forward .
Vin= AC 220V,Vout= DC 27.3V , Iout(max)= 20A,Transformer ratio is 2.5:1, second side filter inductor is 180uH(about 54uH@20A),
Cout=470uF×4(ESR is 54mohms each Electrolytic capacitor)。
Problems :
Below is the wave of Vds, when Iout = 2A. It looks worked not very well.
The compensation part of the schematic is as belows:
I can't get better results through tuning the compensation controll circuit. So ,
Do you have any reference design or technical material about the LM5021MM-2 working in a two-transistor forward converter?
Or could you help tell me how to solve this problem?
Thank you very much !