I am trying to test the bq24650EVM development board as per the user manual but am seeing two issues:
- when I test J2(V(OUT)) on step 2.7.1 the voltage is 12.6V.
- When I do step 2.7.3 (load #2 at 8V) I do not see 0.2A going through the load.
I have a bit of confusion load #2 as I do not have a An HP 6060B or equivalent, so I am using a power supply that has reverse polarity protection. When I did not get the results I was after, I tried using a resistor that would deliver 12.6V at 0.2A of current but did not happen. Additionally, LED STAT1 illuminates regardless of load connection. Can someone let me know what kind of load I can use instead and/or where the problem may be?
Thank you in advance.