All,
I am working on getting a small LCD inverter going. It uses a (TI) TL494C into a full bridge and a couple of 09N05 power transistors to a step up transformer. This is the sort of unit that would go into a tv or laptop to power the backlight. All I want to get out of it is a reliable HV power supply. I see 12V on the VCC, 5V on the regulated power supply, and a clean 3.8V sawtooth wave on pin 5. The circuit is set up to output on the output driver emitters thus the collectors are tied to VCC. However, there is no output whatsoever on pins 9 or 10 and thus no voltage produced from that point on. I am convinced the board is undamaged and working as an identical one does the same thing. Is there something on the TL494 that needs some sort of bias or external voltage applied to make it work. Alternatively is there an inhibit function that would suspend gate drive output unless some bias were applied. My experience with this device is that once connected it just runs.
Thanks
Tom