ISSUE:
Low Power shutdown (UDIM pin L-->H) create delay , something like 4mS in the customer application.
We think the delay is related to the time COMP pin (100nF) to reach it's nominal level regulation
Needs:
1) Reduce or avoid this delay
2) Is there a different/better way to turn off the device and freezing the state?
3) Is there a different/better way to turn ON the device with fast speed up?
4) Is it possible to increase the output current with external device or buffer like half bridge driver + FETs??
Thanks
Best regards
Mauro