Hi,
During 2Phase operation, if the protection operation works only on the slave side to stop the switching operation, will it also stop the master side?
Also, after clearing the slave fault, will it automatically reboot?
Similarly, please tell me what happens when the protection operation works only on the master side.
"protection operation" is taken into account of thermal shutdown and OCP.
If a malfunction occurs inside the device (FET or control circuit etc.) with either Master or Slave, can it stop the other switching?
Best regards,
Yuto Sakai