A customer using the TPS65930 device to power up the OMAP3530 processor. He is using 4.3V as the input voltage to the TPS65930 device including this as the inputs to the 4 external LDO's. The TPS65930 device power up and the three switchers come up OK at 1.2V , 1.2V and 1.8V. Two of the external LDO outputs also come up; VMMC1 = 3V, and VPLL1 = 1.8V. However the other two LDO's, VAUX2 and VDAC are zero volts. The REGEN pin is floating on this design. Can you say why these two LDO outputs might be at zero volts. This is on more than one board.
Thanks,
Faizul Bacchus.