Other Parts Discussed in Thread: LM25145, LM3150
Hi guys
Do we have this DC/DC converter product:
input: 10~25V;
output: 3.3V 5V;
load: 12A;
Converter is better. if not, controller is also OK.
Thanks
Vincent
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Vincent,
Webench returns only controllers. I would start with LM3150 or LM25145.