Other Parts Discussed in Thread: LMV431, , TINA-TI
I need a circuit to limit the voltage excursion in an A/D input. The A/D alowed input voltage range goes from -0.1V to 1.9V. Below a draft of the circuit I am thinking of to solve this need:
The use of the reference on the right side is straightforward. My question is if it is OK to use the TLV431 (or LMV431 for that matter) like the left size i.e. with the anode floating. I am aware I would need to use a 1uF capacitor for each (the draft was drawn with LMV431 in mind).
Thank you in advance.