This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5520: Varying LED string lengths ok?

Part Number: LP5520

We are planning to use the LP5520 for a different application than what it was designed for. I have three white LED strings that have varying number of LEDs. 

CH1: 5 LEDs

CH2: 4 LEDs

CH3: 3 LEDs

Each string will be operating between 2 and 10mA, which should put the output voltage around 10V to satisfy CH 1 (the largest string). The goal is to keep voltages low, and we don't need a lot of current to achieve the desired brightness.  We plan to operate in Adaptive Boost Mode and functionally in Manual Mode, using a microcontroller to interfacing with the LP5520.

Will the uneven string lengths be a problem or do the individual current drivers handle this?

Additional information: We plan to operate on two NiMH cells, and will have to use a boost converter to feed the LP5520.

Thanks,

Leif

  • Hi, Lief,

    It's not a problem for uneven string lengths. The driver adjust the current and different channels will have different drop since the LED number is not the same.

    Please help to click "Resolve" if the problem is solved.

    Thanks.
    Regards,
    Kenneth