This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23610: BOOT-SW shorted

Guru 16770 points

Part Number: LMR23610

Hi

Our customer has the following question.

In case that BOOT to SW is shorted, could it be led to device damage while operating?

As the configuration, Input=24V, Output=3V/0.3A.

I suppose that the device would not be damaged because the voltage for high side gate driver would not be supplied and the device would not work.

Is it correct?

Or could it be possible to lead to device damage?

BestRegards