I would like to have the option to 'select' between 5A charging and 10A charging by changing the ISET1.
I will be charging 1 cell (3,6V) and have an input voltage of 12V
Questions:
1. CAN I use the components selected for 10A also for charging with only 5A ? (Lo = 4.7uH and Co = 30-40uF )
2. And if so, what are the consequences? Will efficiency be less (or more) when charging 5A with a 4,7uH inductor?
3. with 4,7uH, I can use Co=30uF resulting in 13,4Khz resonant freq OR Co = 40uF resulting in 11.6Khz which is better and why?
Thanks in advance for the swift reply.