While using the current monitoring analysis i am looking for IC which will helpful for me to design a the relay controller board which is useful in such a way that whenever current sensor detect unwanted readings either it is high or low then signal will be send to relay board and It will shut down the power of these boards which is used with water pump, other industrial machines to make them preventive from damages,
Note: for monitoring analysis I am using Current sensor with IOT interface board store.ncd.io/.../ and the design I want to work with these kind of sensor should related to I2C wired connection protocol. Its something new an creative for me so for making it much more perfect your great suggestion and advises will be much appreciated.