We have been running charge/discharge cycles to test and understand when State of Health is updated, and have noticed an anomaly:
With three back-to back charge cycles, the SoH is updated each time. However, on two of the three cycles, the Full Charge Termination bit (FC bit in Alert Configuration Register ) has not been set. However, in each of the three cycles, OCV taken occurs properly after charge termination. Can you explain why the FC bit would not get set yet a post-charge OCV is obtained?
These are on Lead Acid batteries, 12v AGM with 105ah capacity.Thanks in advance!