Other Parts Discussed in Thread: TPS65381A-Q1
Hi E2E,
This is my first time to use the TPS65381 and TMS 570. I meet a problem with TPS65381-Q1 and TMS570. I was doing functional test on the board , I found that the system will failed to start up if IGN signal is switched on at the same time as 12V power supply. I studied the data sheet of TPS65381.I have been confused about the discription of " Power-Up and Power-Down Behavior ".
1st. If the IGN signal is lasted high before the start-put of VBATP + 12 V and be pulled down before the end of ACTIVE STATE, the system will be failed to start up and stepp in STANDBY STATE, even the Device State step in STANDBY STATE again? Or the IGN signal could start up the system in more chance?
2nd. If the IGN signal is high before the start-up of VBATP + 12 V and lasted high before the end of ACTIVE STATE, the system will be successed ?
In summary, is there a problem with on-grid timing? If the system fail to start up, I need to use the MCU to clears IGN_PWRL bit?