This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to determine the grade of the TI active components viz. commercial, Industrial or Automotive.

Other Parts Discussed in Thread: TL431

Dear Technical Team,
Good day!!!
Request to please  notify how to determine  the grade of the TI active components,  viz. commercial, Industrial or Automotive.
Regards
Atul Mishra
  • Hi Kumar,

    There is 2 ways.

    Orderable device number.
    Example: TL431BQDBZ
    Family Name:TL431
    Accuracy Grade: blank (2%) , A (1%), B(0.5%)
    Temperature Grade: C(0C-70C), I (-40C to 85C), Q (-40C to 125C)
    Package: DBZ (sot23-3), ect.

    The 2nd way is to checkout the device marking.
    For example on TL431 on the datasheet in Package Option Addendum starting on pg 41 it shows the device marking which will be the top mark of the device.

    -Marcoo