Hi,
I am working in a "GSM based vehicle tracking system ". The circuits are powered by a build in Li-ion battery. Now i need a charger circuit for 3.7V Li-ion battery. The charger circuit will be connected to the vehicle battery (It may be 12V or 24V).
specifications and requirement:
3.7V/1400mAH Li-ion battery
Output load - 2A continuous.
Charger input - 9V to 25V
Cost - Below 2$ (For 10K volume)
Package - (T)QFN not preferred
The IC should have automatic charge ON/OFF control.
How to choose (or what should be) the output voltage of charger IC for 3.7V battery (may i use 4.2V output IC like BQ24075), because the datasheet provides only the output voltage and not the battery rated voltage.
what should be the current capacity of the device if the battery is 1400mAH.
Sorry i don't have any experience in battery charging. So please advice me to select a good charger IC.
Thanks®ards
Udhaya kumar.A
SPECTRUM Embedded Solutions