This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: LP8860-Q1 B Version channel& Blink

Part Number: LP8860-Q1

Dear E2E:

i used LP8860-Q1 B version  ,my load is : 4channel led , ten leds for each channel.   tatal current is 500ma  & Boost Voltage: 32V
But i  was a little confused when checking the  eeprom  version configuration.   Does is suitable or not ?

Actually, the sample was finished,  Basic function is ok in 25℃ condition.  But when i do high-low temperature  test ,the TFT back light screen blink all the time when temperature reach 85℃ 
the schematic as fellow. may i know some advise how to check the circuit. thanks a lot.