This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EM1402EVM: Queries on EM1402EVM

Genius 5355 points
Part Number: EM1402EVM

Hi Support,

Some questions to the evaluation board EM1402EVM below.

1)      per cell spec is 3.6V 30Ah

2)      cell pack connected in series of 8S1p = 28.8V 30ah

3)      For cell balancing I have to connect 8 wires to each cell. Since EM1428EVM is 16 channels cell balancing, how should I connect with 8 cells balancing?

4)      During charging my charger is set to 30V with current is 30A to 60A. Will the large current of 30A to 60A damage the eval board Eval board has stated Vmax is 60V, but it has not stated the max current of charging?

Thanks.