This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Inquiry for 250W Buck PFC

Other Parts Discussed in Thread: UCC28600, UCC28061

Hi,

There is a PFC inquiry for aviation application. Could you kindly give a suggestion what PFC device is suitable for this? Very thanks.

SPEC:

Vin: 90~150 Vac

Vout: 28 Vdc

Iout: 8.9Amp

Watt:250W

Line Frequency (Vin): 62Hz~800Hz

Brian.