Other Parts Discussed in Thread: LM5066, LM5069, TPS2660, TLV333
Hello everyone,
I'm currently working on the LM5066i, especially trying to switch a load with it. I'm using the attatched circuit with two SIR870ADP as switching FETs like in Application note SNVA673 to prevent reverse current.
Turning on seems to work fine. The input is 29.5V and can be measured on the outside as well, even when a load is connected. Unfortunately the output voltage labeled POWER on the right acts strange when turning off the device via the UVLO/EN Pin. Without any load connected, the voltage stays at ~28.6V. When connecting a 470 Ohm resistor, the voltage drops to ~9.1V. The output voltage is also ~28.6V when the LM5066 is turned off, the resistor is connected and then again disconnected. So it cannot be any charged capacitance on the output. The output signal POWER is connected to a pin on a connector and nothing else.
My first thoughts about why the circuit is not working are the two MOSFETs, like in SNVA673. In this application note, the LM5069 is used which differs from my used LM5066. But as the function seems to be similar, I do not know it this is really the reason.