Tool/software: WEBENCH® Design Tools
The problem is that the BQ40Z50-R2 switches and lights can only be controlled independently, and the switches we need to match the Led function as follows:
1. The soft start of the system can be realized by long switch.
2, during the charging process, LED can display electricity for a long time.
3, through the short press button, let LED display electricity;
4, the battery capacity is 10%, LED flicker
Now the function of buttons and LED can not be controlled each other.