Part Number: UCC28070
Hi,
UCC28070 spec shows "Due to the influence of the synchronization pulse width on the programmability of the maximum PWM switching duty cycle (DMAX) it is recommended to minimize the synchronization signal's duty cycle." The max duty cycle is 50% typical, 0.2us min pulse width.
As we will use external clock sync function, please clarify the details influence. If the sync clock follow both 0.2us min width and 50% max duty cycle, whatever Dmax setting value, is it no issue absolutely? Thanks.