Dear Sir,
I don't want to use Host to control BQ24195. once adapter is removed I will put high the OTG Pin to keep SYS 5V.
can I keep folating of SCA/SDA? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Lucifer,
You may leave the SDA and SCL pins floating or short them to GND.
However, do note that the OTG mode does not regulate the system voltage. It only regulates the PMID pin.
Regards,
Joel H