This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25120A: what is the maximum current can be "sourced at the same time" for BQ25120A?

Part Number: BQ25120A

Dear Sir/Madam,

Can i know hat is the maximum current that can be "sourced at the same time" from this IC? Are the following and therefore, the system can deliver a total of 700-mA to the loads in total (Isw + IPMID +iLS/LDO = 700 mA)? 

Best regards,

kpk

  • hi Poh,

    from the battery only mode, you can pull upto 850mA (BATOCP) limit. When VIN is present it can be ILIM current setting + BATOCP limit. I see where the confusion is. I will fix the datasheet to clarify better.

    regards,
    gautham