This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24450: BQ24450 24V Lead Acid Battery charger circuit Resistors Value

Part Number: BQ24450


Hello all,

I need an urgent answer and I will be really glad if you help me please. Can you please suggest me side component values for BQ24450?

I am designing a chrager for valve regulated lead acid battery. I will connect 2 batteries in series and therefore I need to charge them serially. 

Specifications for 1 battery is as below;

Standby Voltage=13.5-13.8V

VBOOST=14.4-15V

IMAX-CHG=3A

VTH=21 for double battery in series

Thank you very much in advance

Kind regards

Ahmet