Other Parts Discussed in Thread: TPS62290, TPS62060
Hi
My Customer has question.Please cooperate me
Customers plan to use them with the following specifications.
■①
VIN:3.3V
Vout:1.8V
Iout:100mA~300mA
■②
Vin:3.3V
Vout:1.2V
Iout:300mA~600mA
The SW frequency of each can be judged from the following figure 17 and 18 as follows.
①Fsw≒1.25MHz
②Fsw≒1.5MHz
Could you tell me the accuracy of the frequency at this time?
It is necessary for the customer to check whether the SW frequency falls within the specified range as the judgment item of good item or defective item of the actual machine.
It may be the accuracy of the internal oscillator, so could you tell me?
Best Regard
T Kishi