Hi,
I am currently building a micro controller circuit that uses a TPS70950 to supply the 5V that the processor needs. I read the spec sheet but still have questions concerning the input capacitor. The specs state that no input capacitor is needed but suggests using a 0.1 to 2uF capacitor installed right next to the regulator.
The circuit I am building uses a power brick that is plugged into the wall. I usually use a diode, for polarity protection, and, say, a 470uF capacitor and sometimes a 0.1uF monolithic, in parallel, installed right next to the input power connector on the board to filter out any noise or ripple. From there, I plan on tapping off some of the input voltage to supply the TPS70950 and micro controller.
My question is, how do I coordinate the global input capacitors with the input capacitance requirements of the TPS70950? Are the 2 sets of capacitors separate and distinct, or do they need to be separated by, say, an additional diode? I don't know how to address this issue.
If anyone has experience with this I would appreciate some guidance.
Thanks,
Dave