Other Parts Discussed in Thread: TPS562208, , TPS562201
Hi Team
When the inductance is too low, high side mode will always turn on and low side MOS always turn off , and this time , Vin will equal Vout
Test condition:
Vin=12V
Vout set to 3.3V
L was originally 2.2uH, but replace wrong value to 0.7uH,
find out Vin is equal Vout,
my customer would like to know what is reason?
By the way
TPS562208 and TPS562209 both has the same situation
TPS562201 is still normal if L replace to under 0.5uH.