This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: EVM interfacing to PC USB without EV2300? Direct I2C communication using MCU?

Part Number: BQ25895
Other Parts Discussed in Thread: EV2400, BQSTUDIO,

Team,

Could you please confirm the below?

-In order to interface with a PC via USB to the BQ25895EVM-664 then an EV2300/EV2400 is mandatory. Correct?
Or is there a way to directly interface to the USB D+/D- pins of the BQ25895EVM-664 to connect to a PC directly?

-I assume that any I2C compatible MCU (with an I2C Master capability and correct IO levels) can interface to the BQ25895EVM-664.
Do we have some code examples to interface via I2C to read/write the register? Example for MSP432 or CC26xx or other TI MCUs?

Thanks in advance,
Anthony